Lead-free RSS

Cable glands, Lead-free, Skintop -

Lead-free: At the petrol station, we have long since become familiar with the fact that petrol is no longer allowed to contain lead. Metallic materials, such as brass, must also dispense with lead as an additive for easier processing – with one exception: Up to four percent is permitted in copper alloys – including brass, which is used to produce cable glands. As things stand, this exception will expire on July 21, 2021, and it is still unclear whether there will be an extension or a transitional period. If the exception ends as planned, brass will no longer be allowed...

Read more